Part Number: ISO1212
This is with reference to figure 3 & 4 in this note. Can the photo transistor idea for power reduction be used with bridge rectifier design for AC inputs? If yes is any reference design available?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rushabh,
Thanks for reaching out.
Yes, the photo transistor idea for power reduction can be used with the bridge rectifier design for AC inputs. We do not have a specific reference design schematic for this circuit, but you can refer to the diagram below to see how this circuit is connected.
Regards,
Kenneth