Hi Sir,
as the datasheet "Isolated RS-485 Transceiver Reference Design" "SLLA453–May 2019"
I want to confirm the circuit full-duplex compatible with half-duplex or not?
I have RS422 full-duplex schematic as below and confirmed with TI FAE but we will chnage application to RS485.
The RS485 should be half-duplex protocol?If yes, I need to modify the schematic to half-duplex?
Thanks
file:///C:/Users/11005077/Desktop/RS422.jpg