Part Number: ISO6760
Dear team,
When I read datasheet of ios6760, I figured out our datasheet showed two different Vcc1 on line 1 and line2. Same as VCC2 on line 3 and 4. Can you help explain why? Thanks!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO6760
Dear team,
When I read datasheet of ios6760, I figured out our datasheet showed two different Vcc1 on line 1 and line2. Same as VCC2 on line 3 and 4. Can you help explain why? Thanks!

Hello Zoe,
This is a minor error on the datasheet. The 1st row is for the recommended operating conditions when Vcc1 = 1.8V and the 2nd row is for when Vcc1 = 2.5 to 5V. The same pattern goes for Vcc2 on lines 3 and 4. The table normally looks like the datasheet for ISO672x attached below.

Sorry for any confusion this has caused. I hope this clears things up.
Best,
Andrew