Part Number: SN6507
Hello
I have a question about the SN6507 Rdc Equation .
SN6507 Equation 1.
RDC = 0.816 × D × VCC × RCLK + 1 − 1
SN6507 Datasheet 22page.
" To achieve maximum input compensation, the DC is set close to 0.25 (25% duty cycle) at typical VCC (24 V).
The RDC is calculated as 240 kΩ by substituting DC = 0.25, VCC = 24 V, and RILIM = 50 into Equation 1, where
both RILIM and RDC are in kΩ. "
Rdc cannot be obtained from this content.
Should Rilm be modified to Rclk ?
I have one more question.
What is SSM and how to disable SYNC Mode?