Hi team,
I have a problem about adjusting switching frequency "Fsw" of SN6505. It is known that it operates between 100kHz to 2Mhz. However, when I placed a 111k Ohm resistor between CLK pin to GND. Driver does not work.
I have tried with 30k, 40k and 50k Ohm resistors for between CLK to GND pins. Results are same: Driver doesn't work.
When I shorted CLK to GND or placed 9.6k Ohm resistor, it works properly at 1.07 Mhz as it mentioned in datasheet.
I want to adjust Fsw to 105 kHz. Is there anyone who can help me?
Regards,