Other Parts Discussed in Thread: ISO1641
Why are the maximum load capacitance and load current ratings for Side 1 of the ISO1640/ISO1641 less than Side 2?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The ISO164x is designed to isolate one I2C node from the rest of the I2C bus. As a result, it has been designed such that Side 1 of the device is to be connected only to one node, while Side 2 is designed to be connected to multiple nodes. Since this is the case, Side 1 has a sufficient load current and load capacitance rating for only one device, while Side 2 has much higher load current and capacitance ratings to support multiple nodes.