Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7720-Q1: isolation rating

Part Number: ISO7720-Q1
Other Parts Discussed in Thread: ISO7720

Hi team,

For ISO7720, it’s descripted 5000V rms isolation rating, it means 5000*1.414 V DC isolation rating, right?

Thanks,

Scarlett 

  • Hi Scarlett,

    Thanks for posting your question on E2E forum.

    We perform our high voltage testing with AC waveforms (rms or pk values). We have noticed that DC voltage is much less stringent on the isolation barrier than the AC voltage and therefore I expect ISO7720 to comfortably pass 5000*1.414 DC voltage stress.

    Thanks,
    Saleem Marwat