Part Number: SN6507
In d/s, it addresses the thermal shutdown threshold is at 184degree,typical, however, the device's junction temp is 150degree. is it making sense? Customer afraid that device could be damaged or injured when TJ>150degree.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN6507
In d/s, it addresses the thermal shutdown threshold is at 184degree,typical, however, the device's junction temp is 150degree. is it making sense? Customer afraid that device could be damaged or injured when TJ>150degree.
Hi Brian,
Thanks for reaching out.
Please note that thermal shutdown is a protection feature to protect the device if its junction temperature exceeds its maximum rating. Hence, thermal shutdown threshold has to be set outside the operating range.
It is expected that the device is always operated under its maximum junction temperature for normal operation and occasionally if there is a fault in the system that causes the junction temperature to exceed its maximum rating, then the thermal shutdown feature can protect the device and avoid any damage. Such use of device is not an issue and you shouldn't have any problems.
Let me know if you have any further questions, thanks.
Regards,
Koteshwar Rao