What’s the difference between Single Protection and Double Protection rating in UL 1577?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What’s the difference between Single Protection and Double Protection rating in UL 1577?
Double Protection isolators need to pass 2 additional tests when compared to Single Protection isolators.
Single protection isolators are required to pass the following 3 tests:
1- Dielectric Voltage-Withstand Test
2- Overload Test
3- Limited Thermal Aging Test
Double protection isolators need to pass the tests above and the following 2 additional tests:
4- 20 kV Discharge Test
5- 1008 Hours Isolator Life Test
Additionally, UL restricts the use of Double Protection Isolators to equipment rated up to 250 Vrms whereas Single Protection Isolators can be used in equipment rated up to 600 Vrms or dc.