Other Parts Discussed in Thread: ISO7741-Q1,
Hi Expert,
Thanks a lot for your warm help.
My customer is using ISO6741- Q1 in their project.
- Here is a question raised by OEM, if the working voltage of ISO7641 of reinforced could meet the 1000Vrms requirement?
Attached is the document they download from ti.com. The working voltage of reinforced insulation is 800Vrms, which
is different from datasheet.

From my perspective, the ISO7741-q1 with DWW package and the creepage is larger than 14mm, which will meet the requirement of OEM.
If we can meet the 1000Vrms requirement, would you mind helping to change the document to eliminate the understanding?
Looking forward to your reply!
Kind Regards
Imelda