This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using this part in an environment where the DC common mode floating voltage incident on the chip inputs can go up to 1500V. There can be about 200 units connected on the RS485 bus. My queries are:
Hi Santanu,
Thanks
Vikas J
Vikas,
Thanks for the reply - really helped. Just wanted to clarify that the 1500V I was talking about is with reference to the floating ground connected to each unit. The ground voltage difference between the first and the last unit connected on the bus can go upto 1500V. What happens if the voltage difference exceeds 1500V (a rare possibility but can happen)
Hi Santanu,
The floating ground connected to each unit will support common mode voltage of -7V/12V wrt to GND2 and device gets damaged beyond ±18V. Hence, you cannot use ISO1410 in your application.
May I know the application in which bus common mode goes up to 1500V?
Thanks
Vikas J
Vikas,
The application is an aluminium smelter where there are about 300 pots (an electrolytic unit) in series. Each pot has a controller and the voltage generated from the pot is about 5 volts. Therefore, the potential difference between the first and last pot is about 1500V even though the voltage difference between adjacent pots is about 5V
Hi Santanu,
Thank you for the information. In my knowledge, none of the RS-485 bus or devices support this unusual requirement. ISO1410 is one of the robust devices for isolated RS-485 communication.
May be a block diagram with voltages mentioned at nodes will help us resolve your concern better.
Thanks
Vikas J