Part Number: ISOW1044
Hi,
I'm looking for replacement part of IL41050. I would like to use it for 1Mbps. Is ISOW1044 OK for this application ?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alikaan,
Thanks for reaching out.
Yes, ISWO1044 can be used as a replacement device for IL41050. Please note that IL41050 is an isolated CAN transceiver without any DC/DC converter integrated and requires external isolated power supplies. While ISOW1044 is an isolated CAN transceiver with integrated DC/DC converter. I understand that you are looking for a device with integrated power, ISOW1044 should meet your requirements.
Let us know if you have any questions, thanks.
Regards,
Koteshwar Rao