Part Number: ISO7720
Hi ,
Just want to check on Min pulse width.Thanks
BRs
Given
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Given,
Thank you for your question. We don't have a defined minimum pulse width, but we can approximate from the data rate. The ISO7720 supports a maximum data rate of 100Mbps, which corresponds to 50MHz signal. That means the signal would have a total period of 20ns, and with a 50% duty cycle, the pulse width would be ~10ns. Therefore it is recommended to use a pulse width of 10ns or greater.
Regards,
Darrah