Part Number: ISO6721
What is the difference between ISO6721 and ISO6721B
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Anna,
Thanks for reaching out.
The letter 'B' indicates that the device is a Basic Isolation version of the original device ISO6721 which is a reinforced isolator. The definition of basic and reinforced isolation according to VDE 0884-17 or IEC 60747-17 is that any device that supports a Surge rating (VIOSM) of >10kV is rated as reinforced isolator while device with <10kV VIOSM are rated as basic isolators.
I hope this answers your question, thanks.
Regards,
Koteshwar Rao