Other Parts Discussed in Thread: ISO1410, SN6501, SN6507
Hi,
Good Day.
I am designing Isolated RS485 circuit for 8 sensors. Following are the requirements
1) Output voltage for RS485 transceiver (isolated side) and for sensor loads: 5V
2) Output current for RS485 transceiver (isolated side) and for sensor loads: 150mA + 100mA for eight sensors
3) Output power switching control
4) Data rate for half-duplex, isolated RS485 transceiver: 19.2kbaud
5) Logic IO voltage (CPU side of RS485 transceiver) is all 3.3V LVTTL
6) Consider EMI / ESD
7) Consider switchable termination (desired but not must)
8) Input voltage range: Either 4.6VDC or 6.5VDC
9) Consider pin reversal capability for RS485 transceiver (A/B) pins (desired but not must)
Could you please suggest integrated solutions such as ISO1176T or other solutions such as ISO1410 with external isolated DC-DC converter ?
Please advise. Thank you very much.
Best Regards,
Ray Vincent