Other Parts Discussed in Thread: ISOW7721, ISO7740, ISO7720, ISO7730
Dear TI experts,
My customer considers ISOW7741 for their new product.
they plans to use 2 ISOW7741 at the same time, because output current of 1 ISOW7741 is small for their application.
in this case, they are wondering that it is necessary to use D1/D2 diodes to protect reverse current.

or does ISOW7741 have some protection circuit like diode itself? then my customer don't need to use D1/D2 diode.
Please check this issue. Thanks.
Best regards,
Chase