This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6741: Question about minimum SPI Frequency

Part Number: ISO6741
Other Parts Discussed in Thread: ISO7741

Hello, 

I am selecting a device to isolate the SPI signals between two MCUs on different boards and I was thinking of using the ISO6741. My design will run at a maximum clock speed of 12MHz at 3.3V and while in the ISO6741 datasheet I could not find any information on minimum SPI clock frequency, in a document called Isolating SPI Signals there is a table in which it is stated that for ISO6741 the minimum SPI clock frequency supported (at 5V) is 13.9MHz. Does this means it is not adequate for my design? What would be an valid alternative in this case?