Part Number: SN6505B
Other Parts Discussed in Thread: SN6501, , SN6507
Hi team,
Recently my customer is evaluating SN6501 and SN6505B, some questions about protection and safety came up. Could you pls help with these questions? Thanks a lot!
SN6505B:
1. how soft start works when power up? In datasheet, the description is "Upon power up or when EN pin transitions from Low to High, the gate drive of the output power-MOSFET is gradually increased over a period of time from 0 V to VCC." So how the device control the gate voltage or gate current? when power up, a single high-current pulse may be applied on output MOSFET, can the device suppress it and protect the MOSFET?
2. About 1.7A current limit, is it an average current limit of output current? what will the device act when overload? When the capacitive load is heavy, what is the maximum current that the device can afford when power up?
SN6501:
1. SN6501 don't have soft start, so how the device protect itself from inrush current when power up?
2. What'll happen when overload?
3. What's the design guide when considering safety and protection?
Thanks!
Rayna