Part Number: ISO7820
Other Parts Discussed in Thread: ISO1412, ISO1042
There is a request to have a design with 50 differential channels from a scsi connector out to another connector.
The signals are asked to be isolated.
Initially, only thinking we wanted straight isolation, we looked at the ISO7820.
As time progressed, additional request came in.
Question: What is a best device for this application? Requirements: Differential, Bidirectional, multichannel, 3,3V