Part Number: ISO1050
Hello! I have a question to ask for advice
Using F2803x CPU and ISO1050DW, for the CPU, CAN is full duplex, while for ISO1050, is it half duplex?
We found a small probability of frame information loss, where a node cannot receive one frame of data from the bus before sending the message, and the two frames of information appear continuously on the bus
Is there a situation where two nodes simultaneously send a frame of information? When ISO1050 of node A processes the sending information, node B first preempts the bus. The information that node A is waiting to send is waiting for the bus to be idle in ISO1050, and ISO1050 is currently occupied. Can it receive information from node B correctly? Or will this frame of information be discarded?
Best regard!