My team included this digital isolator in a recent design and experienced a surprising failure mode. We noticed that an mcu communicating through the digital isolator began to smoke and ultimately was destroyed. We detected that a short existed between VCC and ground on the mcu side of the digital isolator which most likely is what fried the mcu. We removed the digital isolator from the pcb and there was no longer a short on the pcb. However, when probing the VCC2 (pin 16) and GND2 (pin 9) pins on the disconnected isolator, we discovered that there was continuity between them.
This suggested to us that the chip failed in a way which caused a short circuit between power and ground. We are unsure of why the chip failed, but the implications of this type of failure seems severe. Is this a common failure mode for this part?