Part Number: ISO1228
Hey Isolation team,
I have a customer evaluating the ISO1228 for a new project and there are a couple of items in the datasheet that we were hoping to get more clarity from you on:
- In Section 9.2.3.1.2 Voltage Thresholds, it mentions that for Type 2 operation it is recommended to use two channels in parallel. Does this mean that there is a limit in current through the individual inputs? Is it correct to interpret this as the device cannot support 8 inputs in Type 2 mode?
- Again in Section 9.2.3.1.2 Voltage Thresholds, it states that a R_THR value of 1.35kOhm is recommended in Type 3 systems for I_L of 3.5mA in sink mode but then Table 9-1 shows that the TYP and MAX R_THR values for this exact situation are 910Ohm and 950Ohm respectively. Is this discrepancy a typo? Which one is correct?
Any guidance you can provide here would be greatly appreciated!
Best regards,
Matt Calvo