Part Number: ISOW7842
Other Parts Discussed in Thread: TPS3710
See TI Case #
CS1985254 Previously submitted.
I am using ISOW7842 in two locations to create a Viso.
In both location the downside Vcc measures 3.312V.
In one location Viso measures 3.717V.
2nd location Viso measures 3.719V.
Both of these Viso values exceed the data sheet specified Max of 3.58V although
the Absolute Maximum Rating of 6V is not exceeded.
Both of the Viso outputs are supplying the part itself and a TPS3710DDCR device
whose operating voltage range is 1.8V to 18V so there should not be an impact
on the TPS3710 but being out of data sheet spec on two devices is unusual.
What impact will the out of spec Viso have on the device itself? Is there an
impact on performance or reliability?