This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thanks for reaching out.
I am assuming that for your application, you will be applying a square wave to the IN pins of the device, and the square wave will operate from 0-24 V at 500 kHz. If this is not the case, please let me know.
Yes, the ISO1212 is capable of supporting a 0-24 V square wave input at a frequency of 500 kHz. The ISO1212 can have set voltage thresholds that can support a signal with a 0 V low level and a 24 V high level. The ISO1212 is also capable of supporting input signals with a data rate of up to 4 Mbps, which is well above the 500 kHz input frequency of signal that you will be applying to the device. Therefore, the ISO1212 should be capable of supporting an input signal with the requirements that you have specified.
Regards,
Kenneth
Hi Alex,
Thanks for the update. If you have any further questions, please let me know.
Regards,
Kenneth