Part Number: ISOUSB111
Other Parts Discussed in Thread: ISOUSB211
We'd like to know what TI solution is able to address USB application as below diagram. Is that ISOUSB111 able to do so?
CPU in the IPC system that is only supporting USB Host side. And there are two scenarios in applications to access USB port from external side.
Scenario 1. External PC to do the software download to IPC/PAC by USB port.
Scenario 2. Insert a memory device on the USB port.
Is ISOUSB111 able to judge if it's host or device on downstream port? Or what suited solution you suggested?
Application: IPC/PAC industrial motion controller