Part Number: ISO7742
Hi team,
I would like to realize a circuit to connect the OUTA pin of ISO7742 and turn on/off the Pch FET as shown below.
The maximum rating of the OUTA pin (Vccx+0.5V) is not exceeded because of R1 and R2.
If I increase the value of R1 and R2 and suppress the reverse current when OUTA is outputting High, will this configuration work?
If so, what is the maximum rating of the reverse current?

Supplementation:
I am using a Pch FET because I do not want to reverse the logic.
Also, we do not want to add FETs to reduce the number of components.
Thanks.