What is Distance Through Isolation (DTI)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is Distance Through Isolation (DTI)?
Please note that all definitions and references are based on the latest standard IEC 60747-17
Definition:
DTI – Distance Through Isolation. The smallest distance between two voltage domains in the isolator internal to the isolation package
From which certification/standard is this specification derived:
Various standards define DTI. IEC 60747-17 which refers to IEC 60664 to define DTI (IEC 60664 is the Insulation coordination for equipment within low-voltage systems). Please see Distance Through Insulation: How Digital Isolators Meet Certification Requirement for details on each related specification.
How it is specified in TI datasheets:

How it is validated:

Why it matters? Why would I need it? Why would a customer care about this spec?
DTI is the thickness of insulation material and gives a good understanding of theoretical insulating capabilities.
Some end equipment standards may specify a minimum distance through isolation value; however, provisions are included to allow an isolator to become certified if they can pass additional type tests. For additional information please see the related app note Distance Through Insulation: How Digital Isolators Meet Certification Requirement.