Other Parts Discussed in Thread: THVD2450, ISO1450
Hello,
We want to update old components bus based on RS485 to new ones.
Fieldbus is 1 Mbit/s, hard industrial environment (electrical stations). We replaced old driver by new THVD2450, it is running perfecly on our test board. Now we want to remove also our old insulation transformer (with galvanic isolation, ferrite is 16 mH on primary) see schematic, so we hesitate to use ISO1450 wich seems interresting (because it also have galvanic isolation and compact) , do you think ISO1450 can replace our old transformer (galvanic+ferrite)? Should we must add components to target 1 Mbits or ISO1450 is suitable ?
Cordially, Bruno.