Hello TI team,
Can you please clarify following questions:
1. Is there any requirement for minimum recommended pull up resistor value? can we use pull up resistor of 27k, is it fine?
2. We are using this device for DP++, HDMI CEC signal interface isolation, Is it fine?
3. As we require only one section (only SCL is used for HDMI CEC), another section (SDA) pin is open, Is this fine or do we need to connect any resistor for the unused section in and out pins?
4. Can we use this device for HDMI DDC signal isolation, do you see any challenge?
thank you for the support, appreciated
Johnson John