This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Concern,
Please Suggest alternate or Drop in replacement for below mentioned part and kindly provide below details if alternate available.
Part Description |
Original MFR |
Original MPN |
MOQ |
Alternate Available |
Alternate Stock |
Lead time |
Price |
||||
|
|
ISO1176DW |
1000000 |
|
|
|
|
Regards,
Madhav Naik
Hello Madhav,
As mentioned in our previous discussions, ISO1176DWR is an active part with no plans to EOL. (Linking our related threads: (40) ISO1176: Part details Required-ISO1176DWRG4.)
ISO1450DW (Also ISO1410 and ISO1450) is the newest generation device that is pin-to-pin. The only difference is that the "PV" and "ISODE" pins are No Connect in ISO1450DW. This is because ISO1450 has Glitch-Free Power Up and Power Down (10.3.4) and can have the same functionality with just using the DE and RE pins only.
Best,
Andrew