Part Number: ISOW7821
Hi Tier
Could you explain the reason why the load current of VISO pin in 5V to 5V/3.3V condition (130mA) is high than 3.3V to 3.3V (75mA)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOW7821
Hi Tier
Could you explain the reason why the load current of VISO pin in 5V to 5V/3.3V condition (130mA) is high than 3.3V to 3.3V (75mA)?
Hi Tony,
Thanks for reaching out.
The driving strength of internal components is higher when input is 5V due to which the device supports higher current while the driving current is relatively lower for 3.3V due to lower input voltage, the output power that can be delivered by the device is relatively lower.
This is the reason why the output current capability is different for 5V and 3.3V inputs. Let me know if you have any further questions, thanks.
Regards,
Koteshwar Rao
Thank you . But in datasheet the output power is 0.65W. So I think 5* 130mA = 0.65, why 3.3V * 75mA is lower than 0.65W?
Hi Tony,
The datasheet of ISOW7821 specifies that it supports upto 0.65W of power. For 5V input, it supports 0.65W of output power while for 3.3V input, it supports 0.25W of output power.
The explanation I provided in my previous response is the reason for this difference, that higher input voltage enables stronger drive leading to higher power support while for lower input voltage, the drive strength is relatively low leading a relatively lower output power. Thanks.
Regards,
Koteshwar Rao