Dear TI Team,
what does the hysteresis (VCC1) mean, or how should I understand it?

Because if my VCC1 increases from 0V up to 3.3V and the IC can be operated. But if the voltage decreases up to 2.00V will it be turned off because the UVLO threshold hysteresis (VCC1) is 0.2V or must it be below 1.7V? But in this case, why is hysteresis (VCC1) is 0.2V?
I guess the hysteresis (VCC1) value is typical and could vary. Therefore, the difference between 2.25V and 1.7V (the positive and negative-going UVLO thresholds) is greater than 0.2V.
Under these assumptions:
VCC1 from 0V to 3.3V is powered up and will be powered up until the voltage drops to 1.7V and not 2.05V.
VCC1 from 0V to 2.20V is NOT powered up.
How should I understand the power up or down for the state when 1.7 V < VCC1 < 2.25 V.
Regards
Davut Uzun