Hello guys,
One of my customers is considering using ISO6721-Q1 for for level shifting from 2V to 3.3V with isolation.
At this moment, they have the following questions?
Could you please give me your reply?
Q1.
Can ISO6721-Q1 be used for level shifting from 2V at VCC1 to 3.3V at VCC2 though the device datasheet says VCC1 voltage ranges are 1.71V~1.89V and 2.25V~5.5V?
Q2.
If Q1 answer is No, could you please tell me any device which can be used for level shifting from 2V to 3.3V with isolation?
Your reply would be much appreciated.
Best regards,
Kazuya.