Other Parts Discussed in Thread: INA237, , ISO1640, TCA9803
Hi,
We are using INA237 with ISO1641 in our application. Both sides are operating at 3.3V. The side 2 of ISO1641 is connected to INA237 and this part is fine. However, the side 1 of ISO1641 is connected to the I2C master, which is a (non-TI) processor.
The concern is about SDA1 VOL level, which is about 0.57V to 0.71V. Since the processor VIL is 0.66V max. (0.2 x Vcc), we don't have enough margin. The pull-up resistor on the I2C bus is 2.2K. I could increase the pull-up resistor further, but I think the best case margin here would be 0.66V - 0.57V = 0.09V, which may especially not be enough at extreme operating temperature range.
Is there a way we can resolve this issue without introducing any additional part in between?
Any suggestions would be appreciated.
Regards,
Kaitav