Part Number: ISOM8710
HI sir
the ISOM8710 is a right solution in TI to replace HCPL-7720, Thanks
did you have any comptive table?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOM8710
HI sir
the ISOM8710 is a right solution in TI to replace HCPL-7720, Thanks
did you have any comptive table?
Hello Alex,
From a functionality perspective, the ISOM8710 is a device that can perform a similar function, however the 8 pin package and the through hole package are unique for the HCPL-7720 vs the ISOM8710.
Is just a single channel isolated output required for the application?
If so the ISOM8710 would be a great option as it is a smaller package with fewer pins and has simplified control vs the HCPL-7720 as it only needs an input current control to isolate a signal.
Best,
Michael