Part Number: ISOS141-SEP
Does this part experience any SEFIs that require power cycle or is it just transients? Or has no data been collected on this? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOS141-SEP
Does this part experience any SEFIs that require power cycle or is it just transients? Or has no data been collected on this? Thanks
Hello,
Thank you for your question.
Can you please explain what SEFIs are?
If your question is related to radiation tests, the following tests are conducted as stated in the datasheet:
– Total Ionizing Dose (TID) Characterized (ELDRS-Free) = 30 krad(Si)
– TID RLAT/RHA = 30 krad(Si)
– Single-Event Latch-up (SEL) Immune to LET = 43 MeV⋅cm2 /mg at 125°C
– Single-Event Dielectric Rupture (SEDR) Immune (43 MeV⋅cm2 /mg) at 500 VDC
Regards,
Aaditya Vittal
Sure, SEFI=single event functional interrupt. Is there data available on if during SEE test (to LET=43Mevcm^2/mg) there were any transient waveforms or functional interrupts (eg a pin went high or low and was stuck there) that were only solved via power cycle? Or were these types of events not observed/monitored during the test?
Hello Lauren,
Please allow us another couple days to get back to you with more information.
Best,
Michael
Hi Lauren,
Thank you for the additional information.
During radiation tests, the current consumption of the device was monitored to make sure it does not fluctuate to call it a pass. A steady current means that the I/O is not changing and hence, the device was functional during the test.
Please let me know if this is answers your question.
Regards,
Aaditya Vittal