Part Number: ISO1452
How do I configure a RS485 Full-duplex transceiver as Half-duplex?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1452
How do I configure a RS485 Full-duplex transceiver as Half-duplex?
A full-duplex RS485 driver can be configured as a half-duplex driver. However, the Y/Z pins need to be connected to the bus since these are the output (transmit) drivers.
Y/Z pins are the outputs of driver that transmit data from pin D while A/B are the inputs of receiver which receive data from bus and then pass them onto to the output R pin. When full-duplex is used, Y/Z and A/B pins are connected to communication cable separately. While, for half-duplex configuration, Y/Z pins are to be shorted to A/B pins to create one bidirectional bus for both transmit and receive, this is briefly shown in the below image.