Part Number: ISO1450
Other Parts Discussed in Thread: ISO1540, ISO1640,
The purpose of this circuit request, is to create a i2c connection between 2 devices, where the space between the 2 devices is a (NO FLY ZONE)..
I want to build a circuit that is functionally the same as the ISO1540 i2c opto-isolator, but where the 2 halves are on opposite sides of a glass window that no connections can pass through. The 2 circuit boards will be 1 to 2 CM apart, but nothing physical must cross the gap between them.
They will be inside an enclosed metal box that has multiple devices less than 3 inches apart, where each device will be using the same (Optical docking system)
(The plug-in units have their own connector, but there is No physical space for a second connector.)
The backplane will have TCA9548 multiplexer connected side A of the (Optical Dock)
and plugin modules will have side B of the (Optical Dock)
How do I make an equivalent circuit to the ISO1540, where each half is on separate boards?