Dear,
Our customer has some questions about CMTI.
1. According to the datasheet of the CMTI, how to know CMTI test is pass or fail?
I
Below are the test curve, are they pass or fail? I think the first output has inverted due to digital signal, it could be fail, but the second output is almost high, only has one small drop and then changed high, is it pass or fail?
2. The CMTI test need 15pF load. How to balance the small and big Cload? If using the big Cload, the output could be smooth, but if using active probe which could be met the 15pF, but the probe is easy to crosstalk.
3. How to decide the CMTI interference source rise time, the voltage is so defined, such as voltage 100V, time 1ns, Or voltage 2000V time 20ns, this slope is all 100kV/us, but the test results are different, voltage time this is how to consider? In addition, this slope is not the ideal ramp or ramp, how does the oscilloscope take this PASS-capable slope, is it the maximum slope of the segment or the average?
Best regards
kailyn