Part Number: ISO1212
Other Parts Discussed in Thread: ISO1211
HI. I used the component in the STO (safe torque off) circuit.
I am in the process of product certification and need to know if the ISO1212 component has a common point of failure between channels, i.e. that an internal failure on one channel can lead to a failure in the other.
Do you have data or information about it?
Do you think that to achieve SIL3 you must necessarily use an independent single channel device (like ISO1211)?
Thanks for your help
Fabio