Hi team,
In datasheet 6.3 Recommended Operating Conditions, the output current is -60mA to 60mA.
Let me confirm output current. My customer think following condition;
Vcc: 5V
Vout: 2.3V
Load: 54Ohm
Iout = Vout/Load = 42.6mA
So, this is within recommended condition. Is this understanding correct?
Regards,
Youhei MIYAOKA