Other Parts Discussed in Thread: ISOW7742
Hey team,
Just curious, what do we specify as to what will happen if a voltage is applied on the input while the device is Vcc=0? I couldn't find anything in the datasheet except the following which details the off sequence rather than what happens while the device is off.

J&J is seeing that when inputting 4.7V they are seeing 2.5V on the output while the device is off


Thanks,
Cam