Part Number: ISO1412
Other Parts Discussed in Thread: ISOW1412
Hi this is jude from innospace automation.Our application will collect the data from energy meter through rs485 interface.
Here we are using ISOW1412DFMR for RS485 interface.In datasheet Page No 37 - Figure 11-2. The Master GND2 pin is connected with all the devices GND2 pin which is in RS485 network(Image attached
In our design We have to connect the ISOW1412 chip's A and B with energy meter which has only A(D+) and B(D-) line only
Will any communication issue occur, if not connecting the GND2 pin with energy meter
Kindly give me the solution to connect the ISOW1412 with energy meter