Part Number: SN6505B
What are the withstand voltage and maximum current values of the two MOS transistors inside the chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tony,
Thank you for reaching out.
The maximum ratings of the internal transistors are the same as device D1/D2 ratings listed in the absolute max ratings table. i.e., D1/D2 max voltage rating is 16V and the current is 2.4A. Please see below snapshot from datasheet, thanks.

Regards,
Koteshwar Rao