Other Parts Discussed in Thread: ISOM8711, ISOM8110, ISO8110
Hello,
Are there any products that can replace the following products?
・TLP2368
・TLP291-4
Best reagrds,
DDdoor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thanks for looking at our opto-emulators. See my recommendations below:
ISOM8711 is the best replacement for TLP2368.
ISOM8110 is the best replacement for TLP291-4. However, this is a 4-channel device. Currently only single channel options are available.
Best,
Andrew
Hi DDdoor,
Best,
Anderw
Hello Andrew,
Thank you for your support.
Regarding CTR, comparing the specs of ISOM8110 and TLP183, the CTR(MAX) is very different.
For this reason, I am wondering if it is possible to replace it with ISOM8110.
What should I think about this?
・ISO8110
Current transfer ratio (CTR) at IF = 5 mA, VCE = 5V
ISOM8110 : 100% to 155%
・TLP183
Current transfer ratio (CTR) at IF = 5 mA, VCE = 5V
TLP183 : 100% to 600%
Best regards,
DDdoor
Hello DDdoor,
Generally a device with a tighter variance should work in an application with a wider range because the system will have to be designed with consideration for the full range, so a 100-155% should work in applications currently using 100% to 600%.
However, if there is a subset of the range that is generally used, then we are also in progress to release different CTR variants as shown on the datasheet:

A different variant may be selected based on the application need.
Best,
Michael