This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1540: SCL pin receive signal which has platform at the rise edge that will cause low communication rate

Part Number: ISO1540

Hi Ti experts,

We are using ISO I2C ISO1540 to connect MCU and many devices as below:

We found that when ISO1540 receives signals from MCU, there will be a platform at the rise edge as below, which will cause the communication rate down to 300kHz.

Could you please help figure out the reason why there is a platform during signal rises.