Part Number: ISOW7741
On the output side of the isolator, what reference is used for the output enable signal? For example on the ISOW7741 pin 14 is used for enabling outputs on pins 17, 18, and 19. The datasheet in table 7.1 implies that it is referenced to ground on the input side pins 6 and 10 GND1. Is my understanding correct?