This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7721DEVM: Which column in Table F.5 has to be considered for components for IEC 60664-1?

Part Number: ISO7721DEVM


Since TI is using Material group I for all packages for components, it results in less constraints to meet the IEC 60664-1 standard. In order to be sure which column has to be referred to compare the creepage requirement from IEC 60664-1 Table F.5 to the TI component datasheet, could you please answer if it is Column 3 or Column 5 for material group 1  pollution degree 2?