Part Number: ISO1228DFBEVM
Other Parts Discussed in Thread: ISO1228,
hi sir
I want to Design a DI module,I got the TI EVB, I Saw the J3 Connect, so sim tool for ISO1228, or need any dongle?
thanks

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1228DFBEVM
Other Parts Discussed in Thread: ISO1228,
hi sir
I want to Design a DI module,I got the TI EVB, I Saw the J3 Connect, so sim tool for ISO1228, or need any dongle?
thanks

Hello Alex,
Thank you for reaching out.
The ISO1228DFBEVM does not need a dongle to test for normal function. J3 is a standard 2x5 pin connector that is included for convivence.
If you do not have this cable available, the EVM can be evaluated using the J5 or J8 headers.
Best,
Andrew
Hey Alex,
No, currently we do not have sample code available.
Best,
Andrew
Hello Alex,
There is no sample code since the device does not need code. The most basic of the SPI setups is explained in the below datasheet section.

To read from ISO1228:
Best,
Andrew