Other Parts Discussed in Thread: ISO1410
Hello,
We used an old bus based on RS485, and upgrade our equipment to use ISO1430 which works perfectly. We have a doubt about ground, because the "shield wire" is connected to DB9 on our equipment to ground throughout a capacitor and varistor, to have a network to the same equipotential.
To have good 61000 -4-4 tests, should we connect the ground of ISO1430 via the capacitor and varistor (see image, solution 1?), or should we isolate the grounds of the ISO1430 and connect them directly to the ground (see image, solution 2?)
Regards, Bruno